Example MPC5604B Flash Array Integrity Check - using SSD flash drivers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5604B Flash Array Integrity Check - using SSD flash drivers

Example MPC5604B Flash Array Integrity Check - using SSD flash drivers

This is simple example of the usage of Flash Array Integrity Check (FAIC) function that is available on all MPC56xx devices.

 

The FAIC reads data from selected and unlocked flash blocks and calculates the MISR signature. User can compare the MISR signature calculated by flash controller (in runtime) with MISR calculated by offline tool (this is done during development, not in runtime) from s-record file. If the MISR is identical, we know that the content of selected flash blocks corresponds to content in s-record file and that there are no ECC errors (single bit or double bit ECC errors).

标签 (1)
附件
无评分
版本历史
最后更新:
‎10-14-2014 07:19 AM
更新人: