Unable to start Wifi/BT module LBEE59B1LV on IMX8ULP-EVK9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to start Wifi/BT module LBEE59B1LV on IMX8ULP-EVK9

257件の閲覧回数
dhruvinrajpura
Contributor II

I am using IMX8ULP-EVK9 in that currently I want to bring up Wifi/BT on A core, For that I loaded prebuilt image in it and followed IMX_LINUX_USERS_GUIDE with below steps

# For all the Wi-Fi modules:
modprobe moal mod_para=nxp/wifi_mod_para.conf
$connmanctl
connmanctl> enable wifi
connmanctl> scan wifi
connmanctl> services /* This should list of the network. For example
 wifi_c0e4347f5053_4a62726f_managed_psk*/
connmanctl> agent on
connmanctl> connect wifi_c0e4347f5053_4a62726f_managed_psk /* Enter Passphrase
 */
Agent RequestInput wifi_c0e4347f5053_4a62726f_managed_psk
Passphrase = [ Type=psk, Requirement=mandatory ]
Passphrase?
connmanctl> quit

 

I am able to execute all above commads and able to connect wifi with my mobile hotspot as well.

Now we changed Wifi/BT module from LBEE5CJ1XK(In Built) to LBEE59B1LV Type 1LV on the EVK board and again boot-up A core, but in this case while enabling wifi in connmanctl giving error,

connmanctl> enable wifi
wifi is not available

 

So, I want to know that what changes I need to do to start LBEE59B1LV in A core of IMX8ULP-EVK9

 

#nxp #embedded #imx

 

0 件の賞賛
返信
1 返信

224件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @dhruvinrajpura!

The Linux User Guide is focused on our wifi devices.

Unfortunately, we don't have any guide on how to use that wifi module on our BSP in our Boards.

For this case, I recommend contacting Infineon support or Murata support to get the drivers and how to install them on our board.

I recommend using our wifi devices, which are integrated and tested on our boards.

 

Sorry for the mistake!

 

Best Regards!

Chavira

0 件の賞賛
返信