How to use LIN on s32g

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use LIN on s32g

554件の閲覧回数
LB666
Contributor I

How to verify the communication function of two LIN channels on the Linux driver of BSP37 when there are two LIN channels on the S32g274A RDB2 development board

 

0 件の賞賛
返信
3 返答(返信)

517件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @LB666

Thanks for the reply

There are LIN support in RTD SW packages, you may test/modify the examples in it to test the LIN function according to the requirements.

 

Best Regards

Chenyin

0 件の賞賛
返信

538件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @LB666

Thanks for the question

Seems you want to test the LIN under Linux in BSP37? Well, current Linux BSP releases do not include support for the LIN mode of LinFlexD, only UART mode supported in newer BSP versions.

If you want to verify the LIN functions, we suggest using the drivers available in RTD SW packages.

 

Best Regards

Chenyin

0 件の賞賛
返信

528件の閲覧回数
LB666
Contributor I
Okay, so how do I test LLCE-LIN? Can you provide some reference materials
0 件の賞賛
返信