Hello,
I'm using MCUXpresso for VS Code for the first time.
I started by installing a repository, i.e., the MCUXpresso SDK from github.
Then I wanted to import an example from this repository but the LPCXpresso55S36 Development Board seems not supported, see screenshot:
That's strange, as the MCUXpresso SDK clearly contains files for the LPC5536 processor, see here:
https://github.com/nxp-mcuxpresso/mcux-sdk/tree/main/devices/LPC5536
Please advise!
Thanks.
Daniel
已解决! 转到解答。
Hi, danielholala
When I set up the repository, the version I chose was MCUX_2.14.0_LPC55S36. I can find the LPCXpresso55S36 Development Board.
There is another way you can try, You can download the LPCXpresso55S36 Development Board from MCUXpresso SDK Builder, download address for https://mcuxpresso.nxp.com/en/welcome, Note the following Toolchain options, select ALL Toolchain.
Download the sdk in the C:\VS_Code\ SDK_2_14_0_LPCXpresso55S36.zip directory and install a repository locally.
Then, import the LPCXpresso55S36 development board sample.
BR
Xu Zhang
Hi, danielholala
When I set up the repository, the version I chose was MCUX_2.14.0_LPC55S36. I can find the LPCXpresso55S36 Development Board.
There is another way you can try, You can download the LPCXpresso55S36 Development Board from MCUXpresso SDK Builder, download address for https://mcuxpresso.nxp.com/en/welcome, Note the following Toolchain options, select ALL Toolchain.
Download the sdk in the C:\VS_Code\ SDK_2_14_0_LPCXpresso55S36.zip directory and install a repository locally.
Then, import the LPCXpresso55S36 development board sample.
BR
Xu Zhang
Dear @Xu_Zhang ,
Thank you for your support. Somehow I missed the "MCUX_2.14.0_LPC55S36" entry. Following your instructions, I installed this version of the MCUXpresso SDK and now I can select the "LPCXpresso LPC55S36 board" when importing an example.
Note that I ordered the LPC5536-EVK which, obviously, hosts a LPC5536 and not a LPC55S36.
I tried the "led_blinky" example and now see that the device is set to "LPC55S36". Should that bother me?
See screenshot:
Have a nice day.
Daniel
Hello Xu Zhang,
I tried it with a standalone SDK generated and downloaded from SDK Builder.
That does not change anything:
The examples are the same. They are depending on the board that I select and there are only LPC55S36-based boards selectable.