Hello ,
I am intending to use classic CAN module in LPC54606/08 controller.
I tried code generation from MCUXpresso IDE for the CAN module.
But I get a warning while configuring.
Issue: Unsupported version of the MCAN Driver in the toolchain/IDE project. Required: 2.0.1, actual: 2.1.1. Project might not compile correctly.
Level: Warning
Type: Validation
Tool: Toolchain/IDE project
Origin: Peripherals
Target: Toolchain/IDE project: core0
Resource: platform.drivers.mcan
I am using MCUXpresso IDE v11.1.1 [Build 3241] [2020-03-02]
Are the any issue if I use latest mcan driver with the IDE?
regards,
Hemanth
解決済! 解決策の投稿を見る。
Hello Hemanth,
It doesn't matter, you can directly ignore it, the generate code is right.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Hemanth,
It doesn't matter, you can directly ignore it, the generate code is right.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks Alice for the update.
regards,
Hemanth