I am sending a start signal to a device which return nack if it is not ready and ack if it is. I am using the #SDK I2C_MasterStart but it doesn't have a way of returning the ack/nack response from the slave device. Is there another way to do this?
I don't know what happened, but it started sending the correct number of receive bits. And the device CRC matches. I got around the 'not being able to get the ack/nack status' by just waiting longer than the maximum device measurement time. I saw that there was a bit in the master i2c registers that I can possibly read directly.
When I send it with a *write* direction it sends the 9 bits with correct address R/W bit and waits while slave asserts the ack bit (so far so good) . but when I send the same command to the same address but with a *read* direction it sends 17 bits (address, R/W, ack?, 8 unknown bits). I doesn't seem to turn the bus around to receive the return ack/nack bit.