FatFs directories explaination

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FatFs directories explaination

ソリューションへジャンプ
408件の閲覧回数
mastupristi
Senior Contributor I

Hello,

In the SDK for RT1xxx I find the meddleware related to FatFs. It is hosted on github here
https://github.com/nxp-mcuxpresso/fatfs/tree/mcux_release

In there I find some directories that implement abstraction for sd, ram disk, mmc, etc.

dir.png

Can you explain the fsl_usb_disk directory? Where is the filesystem archived? In ram like the ram disk?

 

best regards

Max

 

 

 

0 件の賞賛
返信
1 解決策
385件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

Yes, your understanding is absolutely correct.

Best regards,
Gavin

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
392件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

Thanks for your interest in NXP MIMXRT series!

In the RT series SDK, the fsl_usb_disk is the abstraction layer in the FatFs file system for USB storage devices. Instead of being stored in RAM, the file system is stored on an external storage device connected via USB, such as a USB flash drive or hard disk. When you use `fsl_usb_disk`, it manages the file system on the USB storage device.

Best regards,
Gavin

 

0 件の賞賛
返信
389件の閲覧回数
mastupristi
Senior Contributor I

Hi @Gavin_Jia ,

let me see if I have understood correctly: in this scenario, the RT1xxx microcontroller is usb host, right? And the device is a usb storage stick, right?

 

best regards

Max

0 件の賞賛
返信
386件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

Yes, your understanding is absolutely correct.

Best regards,
Gavin

0 件の賞賛
返信