FRDM-K66F Connect EVK flash loader over UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K66F Connect EVK flash loader over UART

1,960件の閲覧回数
nhitpad
Contributor II

Hi 

 I want to using UART to program the EVK.   But unable to connect to UART for programming. 

Here if the Job I already finish.

1. I Programming the flashloader example into the EVK over Jlink. 

2. I able to connection the EVK over USB port and programming it over KinetisFlashTool.

3. I can programming the FW to the start address as 0xa000 over USB port. 

4. I trying  connect to the EVK over openSDA port  with UART mode and I also can get the COMPORT device form the laptop. But When I try to connect it over serial port it will always show :

        Error: Connect device failed(Error: Initial ping failure: No response received for ping command.). 

The purpose for me is I want to programming the  FW over UART.
PS: 

I check the UART port configuration of the SDK example and EVK schematic is set the openSDA SDK port as PTB16 and PTB17. 

 

Thanks 
Kent Yeh

 

0 件の賞賛
返信
11 返答(返信)

1,949件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Kent Yeh,

Please download the frdmk66f_freedom_bootloader to FRDM-K66F board. Then you should be able to connect the FRDM-K66F with it's UART(OpenSDA J26)

Target Address 0x0000A000.png

The frdmk66f_freedom_bootloader can be found under this folder: \SDK_2_10_0_FRDM-K66F\boards\frdmk66f\bootloader_examples

Best Regards,
Robin

0 件の賞賛
返信

1,929件の閲覧回数
nhitpad
Contributor II

Hi, Robin 

   Thanks for response. I tried with the example code both for SDK 2.9.0 and 2.10. both of them is not available for me. Does there have any JMP I need to changed 

Here is the parameter what I used:

SDK 

 PIC1.png

 

PIC2.png

EVK and connection:

WeChat Image_20220117115302.jpgWeChat Image_20220117115309.jpg 

 

Thanks

Kent Yeh

 

0 件の賞賛
返信

1,924件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please update DAPLink bootloader and firmware (0244_K20DX_FRDMK66F_0X8000.BIN

) of the OpenSDA on FRDM-K66F.

DETAILS.png

Check if serial port of OpenSDA can communicate properly, for example by running a UART routine.

2.4 PC Configuration Get Started with the FRDM-K66F.png

0 件の賞賛
返信

1,911件の閲覧回数
nhitpad
Contributor II

Hi , Robin  

I tried  stop the service and programming the   0244_K20DX_FRDMK66F_0X8000.BIN into the address of 0x0000000 and 0x0008000

      service.png

pic4.png

But still failure.  with device connection:

Could you give me your test Firmware, I can verified is it  hardware issue 

 

Thanks 
Kent Yeh

 

0 件の賞賛
返信

1,888件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

You can direct drop 0244_K20DX_FRDMK66F_0X8000.BIN (firmware application of K20 on FRDM board) into driver of FRDM. I just want to ensure the serial port of OpenSDA(K20) is working well.
After download the frdmk66f_freedom_bootloader to FRDM-K66F board, you should able to connect it by using KinetisFlashTool.

0 件の賞賛
返信

1,875件の閲覧回数
nhitpad
Contributor II

Hi, Robin 

    Could you specific tell me how to drop the bin file into the driver of FRDM.

The attachment is the image what I built on my side

Kent Yeh

0 件の賞賛
返信

1,865件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

About how to drop the bin file, please refer: OpenSDAv2

0 件の賞賛
返信

1,835件の閲覧回数
nhitpad
Contributor II

Hi, Robin 

   I've update the  0244_k20dx_bl_0x8000.bin  file base on the stage of SDA update . 

but it's look like malfunction after update it. I can not power the module after connect the SDA port, 

Could you tell me how I can repair it

Thanks 

Kent Yeh

タグ(1)
0 件の賞賛
返信

1,828件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please tell me the state of your board.

state.png

0 件の賞賛
返信

1,768件の閲覧回数
nhitpad
Contributor II

Hi ,Robin 

  Now it can not be power on when I connect the SDA USB to my lap. 

Therefore. nothing will happen after I press the reset button. 

I also try to give module power over USB port. it can be power on but also without any response on the first stage ( Holding the reset  button then connect to my lap top).

 

Kent Yeh

0 件の賞賛
返信

1,665件の閲覧回数
nhitpad
Contributor II

Base on the operations , the board is crashed. And I can not get any help to fix it now.

タグ(1)
0 件の賞賛
返信