Build Date: 2018-06-18, Device: MK64FN1M0xxx12
OS: Linux, Toolchain: GCC ARM Embedded
Components: CMSIS DSP Library
SDK Version: KSDK 2.4.0 (2018-06-05)
The zip archive is always corrupt, no matter what components I choose. Please help!
Hi,
the problem is in the ZIP file name extension. That is incorrectly added to the packages generated for Linux or Mac OS. Please, change it to tar.gz and proceed with decompressing.
This problem will be fixed on the website early next week.
We are sorry for the inconvenience.
Hello,
Neither the Windows 10 unzip tool nor the Ubuntu Linux archive manager
could open the zip file, but 7-Zip for Windows was able to recover a
single large tar file from the zip. After un-tarring, all the SDK files
were there!
You might want to take a look at your SDK builder, though. It is
frustrating that it is creating corrupted zip files that are not
accessible from the default unzip apps on both Windows and Linux!
Thanks,