when using MCUXpresso IDE, how to download built image to target

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

when using MCUXpresso IDE, how to download built image to target

Jump to solution
198 Views
ygao
Contributor I

Hi,

In the hello world example readme file, it says:

"Download the program to the target board"

How to do it? Is there a download button/menu?

Thanks,

Winston

0 Kudos
Reply
1 Solution
157 Views
AdrianOltean
NXP Employee
NXP Employee

I suggest you start browsing the User Guide. There are sections describing how to import an SDK, how to import an example project from an SDK and also how to build and debug (implicitly "downloads" program to target). There's also a GUI Flash Tool that's quite handy.

Thank you,

Adrian

View solution in original post

0 Kudos
Reply
1 Reply
158 Views
AdrianOltean
NXP Employee
NXP Employee

I suggest you start browsing the User Guide. There are sections describing how to import an SDK, how to import an example project from an SDK and also how to build and debug (implicitly "downloads" program to target). There's also a GUI Flash Tool that's quite handy.

Thank you,

Adrian

0 Kudos
Reply