i.mx 1050 csi examples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx 1050 csi examples

2,630件の閲覧回数
natester
Contributor I

I'm getting the following error trying to load the csi examples in mcuexpresso & the evkb-imx1050 2.4 sdk:

pastedImage_1.png

UnmarshalException

javax.xml.bind.UnmarshalException
- with linked exception:
[org.xml.sax.SAXParseException; lineNumber: 89; columnNumber: 40; cvc-enumeration-valid: Value 'segger_script' is not facet-valid with respect to enumeration '[init, run, linkserver_connect, linkserver_reset, linkserver_erase]'. It must be a value from the enumeration.]
- with linked exception:
[org.xml.sax.SAXParseException; lineNumber: 89; columnNumber: 40; cvc-enumeration-valid: Value 'segger_script' is not facet-valid with respect to enumeration '[init, run, linkserver_connect, linkserver_reset, linkserver_erase]'. It must be a value from the enumeration.]
at javax.xml.bind.helpers.AbstractUnmarshallerImpl.createUnmarshalException(AbstractUnmarshallerImpl.java:335)
at com.sun.xml.internal.bind.v2.runtime.unmarshaller.UnmarshallerImpl.createUnmarshalException(UnmarshallerImpl.java:563)
at com.sun.xml.internal.bind.v2.runtime.unmarshaller.UnmarshallerImpl.unmarshal0(UnmarshallerImpl.java:249)
at com.sun.xml.internal.bind.v2.runtime.unmarshaller.UnmarshallerImpl.unmarshal(UnmarshallerImpl.java:221)
at com.sun.xml.internal.bind.v2.runtime.unmarshaller.UnmarshallerImpl.unmarshal(UnmarshallerImpl.java:276)
at com.nxp.mcuxpresso.core.datamodels.providers.SDKManifestProvider.useExternalExample(SDKManifestProvider.java:1490)
at com.nxp.mcuxpresso.core.datamodels.ui.wizards.SDKImportWizard.doFinish(SDKImportWizard.java:194)
at com.nxp.mcuxpresso.core.datamodels.ui.wizards.AbstractSDKWizard$1.run(AbstractSDKWizard.java:70)
at org.eclipse.jface.operation.ModalContext$ModalContextThread.run(ModalContext.java:119)
Caused by: org.xml.sax.SAXParseException; lineNumber: 89; columnNumber: 40; cvc-enumeration-valid: Value 'segger_script' is not facet-valid with respect to enumeration '[init, run, linkserver_connect, linkserver_reset, linkserver_erase]'. It must be a value from the enumeration.
at com.sun.org.apache.xerces.internal.util.ErrorHandlerWrapper.createSAXParseException(ErrorHandlerWrapper.java:203)
at com.sun.org.apache.xerces.internal.util.ErrorHandlerWrapper.error(ErrorHandlerWrapper.java:134)
at com.sun.org.apache.xerces.internal.impl.XMLErrorReporter.reportError(XMLErrorReporter.java:396)
at com.sun.org.apache.xerces.internal.impl.XMLErrorReporter.reportError(XMLErrorReporter.java:327)
at com.sun.org.apache.xerces.internal.impl.XMLErrorReporter.reportError(XMLErrorReporter.java:284)
at com.sun.org.apache.xerces.internal.impl.xs.XMLSchemaValidator$XSIErrorReporter.reportError(XMLSchemaValidator.java:452)
at com.sun.org.apache.xerces.internal.impl.xs.XMLSchemaValidator.reportSchemaError(XMLSchemaValidator.java:3230)
at com.sun.org.apache.xerces.internal.impl.xs.XMLSchemaValidator.processOneAttribute(XMLSchemaValidator.java:2825)
at com.sun.org.apache.xerces.internal.impl.xs.XMLSchemaValidator.processAttributes(XMLSchemaValidator.java:2762)
at com.sun.org.apache.xerces.internal.impl.xs.XMLSchemaValidator.handleStartElement(XMLSchemaValidator.java:2050)
at com.sun.org.apache.xerces.internal.impl.xs.XMLSchemaValidator.startElement(XMLSchemaValidator.java:740)
at com.sun.org.apache.xerces.internal.jaxp.validation.ValidatorHandlerImpl.startElement(ValidatorHandlerImpl.java:570)
at com.sun.xml.internal.bind.v2.runtime.unmarshaller.ValidatingUnmarshaller.startElement(ValidatingUnmarshaller.java:86)
at com.sun.xml.internal.bind.v2.runtime.unmarshaller.SAXConnector.startElement(SAXConnector.java:153)
at com.sun.org.apache.xerces.internal.parsers.AbstractSAXParser.startElement(AbstractSAXParser.java:509)
at com.sun.org.apache.xerces.internal.impl.XMLNSDocumentScannerImpl.scanStartElement(XMLNSDocumentScannerImpl.java:374)
at com.sun.org.apache.xerces.internal.impl.XMLDocumentFragmentScannerImpl$FragmentContentDriver.next(XMLDocumentFragmentScannerImpl.java:2784)
at com.sun.org.apache.xerces.internal.impl.XMLDocumentScannerImpl.next(XMLDocumentScannerImpl.java:602)
at com.sun.org.apache.xerces.internal.impl.XMLNSDocumentScannerImpl.next(XMLNSDocumentScannerImpl.java:112)
at com.sun.org.apache.xerces.internal.impl.XMLDocumentFragmentScannerImpl.scanDocument(XMLDocumentFragmentScannerImpl.java:505)
at com.sun.org.apache.xerces.internal.parsers.XML11Configuration.parse(XML11Configuration.java:841)
at com.sun.org.apache.xerces.internal.parsers.XML11Configuration.parse(XML11Configuration.java:770)
at com.sun.org.apache.xerces.internal.parsers.XMLParser.parse(XMLParser.java:141)
at com.sun.org.apache.xerces.internal.parsers.AbstractSAXParser.parse(AbstractSAXParser.java:1213)
at com.sun.org.apache.xerces.internal.jaxp.SAXParserImpl$JAXPSAXParser.parse(SAXParserImpl.java:643)
at com.sun.xml.internal.bind.v2.runtime.unmarshaller.UnmarshallerImpl.unmarshal0(UnmarshallerImpl.java:243)
... 6 more

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,356件の閲覧回数
natester
Contributor I

Great, upgrading the MCUXpresso IDE from 10.1 to 10.2 fixed the issue!

0 件の賞賛
返信

2,356件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Can you confirm what version of MCUXpresso IDE you are using? SDK 2.4.0 package should only be used with MCUXpresso IDE v10.2.0 (or later).

If you are using MCUXpresso IDE v10.2.0, can you confirm if there is any warning message displayed in the IDE's "Installed SDKs" view after installed the SDK?

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信