I'm looking for a way to cause the currently opened instance of MCUXpresso to open a file at a specified line. Search tools like grepWin have editor configurations to support executing a command line when a search result is double-clicked. For example, here's the options to do that using Notepad++.
C:\Program Files\Notepad++\notepad++.exe %path% -n%line%
I don't see relevant command line options in the MCUXpresso IDE help feature. Can someone point me to where relevant MCUXpresso command line options are documented?
Thanks!!
It should work that way:
https://wiki.eclipse.org/Eclipse/OpenFileFeature
https://insights.sigasi.com/tech/make-eclipse-open-files-command-line/
Have not tried it with the actual MCUXpresso IDE, but hopefully this is all what you need.
Thanks, but unfortunately your suggestion didn't work for me. Perhaps it's due to something in MCUXpresso. Your suggestion resulted in attempting to open another instance of MCUXpresso, which failed because the associated workspace was already in use by the prior instance of MCUXpresso.
These are the command lines I tried (for grepWin) (ensuring the IDE was closed first).
C:\nxp\MCUXpressoIDE_11.4.1_6260\ide\mcuxpressoide.exe -name Eclipse --launcher.openFile %file%:%line%
C:\nxp\MCUXpressoIDE_11.4.1_6260\ide\mcuxpressoide.exe -name mcuxpressoide --launcher.openFile %file%:%line%
While they both opened the IDE, neither opened a file in the IDE.