command line build run not successfull after first 1-3 tries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

command line build run not successfull after first 1-3 tries

575 Views
l_volkmann
Contributor III

Hello,

we are using a script to custumer board releases.
When starting the build I see the 1-3 times the following output:
Opening 'trunk'.
Saving workspace.
Mcuxpressoide:
An error has occurred. See the log file
/home/l.volkmann/.MCUXpresso/build/b34722ff838183abb6f4923b23234f8b1d7531b318ab408c20a9239d02d9b3ca/.metadata/.log.
With log data:
!ENTRY org.eclipse.core.resources 4 2 2020-05-14 13:47:45.584
!MESSAGE Problems occurred when invoking code from plug-in: "org.eclipse.core.resources".
!STACK 1
org.eclipse.core.internal.resources.ResourceException(/trunk/DAB03 Release/sources.mk)[368]: java.lang.Exception: Resource '/trunk/DAB03 Release/sources.mk' does not exist.
... (java call stack)

It seems to me that the make process starts before the automatic makefile generation has been completed.
Has someone any idea how this can be fixed ?

Thanks in advance
Lutz

Tags (1)
0 Kudos
1 Reply

529 Views
converse
Senior Contributor V

What is you command line?

0 Kudos