I am trying to reset the XRT1160/1170 via software. I have tried a few methods and all have failed
What I have tried so far:
All of them hang the MCU, debugging stops, and it doesn't complete the reset.
This is on a custom board with an IS25xxx QSPI Chip https://www.issi.com/WW/pdf/flash-spi_electronica2014.pdf
Along with the above mentioned attempts I have read through multiple other blog posts to no avail. I have also tried the watchdog example and the reset example, neither correctly reset the MCU.
Any help is appreciated.
Thanks,
Cole
已解决! 转到解答。
I figured it out, the debugger was halting the code. If I disconnect the Debugger it works as intended.
specifically
Works
I figured it out, the debugger was halting the code. If I disconnect the Debugger it works as intended.
specifically
Works