SEGGER J-Link configurations don't show up in MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SEGGER J-Link configurations don't show up in MCUXpresso IDE

ソリューションへジャンプ
2,570件の閲覧回数
laszlomonda
Contributor V

Hi there,

I'm back to firmware development after a long break, and I've just realized that I can't flash firmware with SEGGER J-Link via MCUXpresso IDE 10.3.1 on Linux anymore.

Our project is open source. See the .launch files. I can see uhk60-right_debug_kboot and uhk60-right_release_kboot under External Tools Configurations, but I can't see the uhk60-right_debug_standalone_jlink configuration anywhere, including Debug Configurations and Run Configurations.

When I double-click on the "GDB SEGGER Interface Debugging" menu item of the Debug Configurations dialog, I get a dialog featuring:

"An error has occurred. See error log for more details.
java.lang.NullPointerException"

JLinkExe works from the command line, but I can't use SEGGER JLink from MCUXpresso IDE. Any help would be appreciated.

- Laci

0 件の賞賛
返信
1 解決策
2,392件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I missed to mention that you have to have a project selected:

pastedImage_1.png

You can read the project selected in the IDE quickstart panel (marked in yellow above).

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
2,394件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Laci,

I believe I reported that issue with the NPE already, so I think this will be fixed in the upcoming release.

The workaround (and usual way to create/launch a debug session) is to use the 'blue' debug icon in the toolbar: this will automatically create the correct launch/debug configuration.

Can you try this if this works for your project?

I hope this helps,

Erich

2,394件の閲覧回数
laszlomonda
Contributor V

Thanks Erich!

Unfortunately, the blue debug icon is greyed out for me, even after booting the debug probe.

What NPI stands for?

0 件の賞賛
返信
2,394件の閲覧回数
BlackNight
NXP Employee
NXP Employee

NPI was a type, I wanted to write NPE (Null Pointer Exception).

About the debug icon: make sure you are in the develop perspective:

pastedImage_1.png

I hope this helps,

Erich

0 件の賞賛
返信
2,394件の閲覧回数
laszlomonda
Contributor V

I'm in develop perspective, but the blue bug icon is still greyed out.

Untitled.png

0 件の賞賛
返信
2,393件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I missed to mention that you have to have a project selected:

pastedImage_1.png

You can read the project selected in the IDE quickstart panel (marked in yellow above).

I hope this helps,

Erich

0 件の賞賛
返信
2,394件の閲覧回数
laszlomonda
Contributor V

You're right, Erich! The project was already selected, but the blue bug icon was greyed out. Strangely, I have to open the quickstart panel, then go back to the project explorer, then the icon becomes clickable. This is very weird, but solved the issue.

0 件の賞賛
返信
2,394件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The 'blue' debug icon is linked with the quickstart panel, so you need to have this one open. That's why in the normal 'debug' perspective the blue icon might be disabled too.

0 件の賞賛
返信