Restore debugger - LPCXpresso824 Max

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Restore debugger - LPCXpresso824 Max

1,046 次查看
mlp
Contributor I

Hello, I've used the debugger many times, but now things have gone wrong such that I'm now getting an error message "Failed on connect: Ee(36).  Could not connect to core.  No connection to chip's debug port" and then "error closing down debug session - Em(02). MEM-AP is not selected.

Is there a way to restore the factory settings on the debugger?

I've tried:

 - updating board firmware

 - holding ISP switch down while then pushing the reset button

 - holding reset button in while applying power to board

 - modifying preferences (uncheck "Pull ISP on reset)

Error messages from MXUXpresso IDE attached.

I'm hoping there might be some magic command to reset things to the original state.

Thanks in advance for your help!

0 项奖励
回复
1 回复

763 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

First of all, please ensure that you have no spurious debug executables running, by killing any processes in your task manager matching:

  • redlinkserv
  • arm-none-eabi_gdb*
  • crt_emu_*

Then delete any .launch files from within your project.

[Note - Do not use the "broken" project for this. Use a "blinky" type project, from, for example, the LPCOpen package for LPC824.]

Now remove your LPCXpresso824-MAX board from your computer.

Check whether you have a jumper fitted on header JP1. If you do, this will disable the built in debug probe (and debug definitely won't work through it!)

Now plug your board into your PC. What do you see in Windows "Devices and Printers" or equivalent?

Now press and hold the ISP button (top right of the board), press and release the Reset button in the bottom left, then release the ISP button.

Now select your project in the IDE's Project Explorer view and click on the "Debug" entry of the QuickStart Panel. Does the IDE detect your board, and if so, what exactly does it display?

Assuming you can see your board in the detection dialog, select it, then continue. Does the debug session start correctly? If not, please post the text from the Debug log (debug messages) and redlinkserv consoles (as per section 14.11 - The Console View - of the MCUXpresso IDE v10.0.2 User Guide).

One thing that do you do need to watch, particularly if you have installed new probe firmware, is that you have the appropriate serial port driver install. Either the mbed serial port driver for the old mbed firmware (there is a link to this on the IDE's Help -> Additional Resources menu), or if you have installed the newest firmware, then the appropriate serial driver for that. For more information on the new firmware, see: New debug probe firmware & drivers for MAX boards 

Anyway, let us know how you get on.

Regards,

MCUXpresso IDE Support

0 项奖励
回复