Hi All
Does anyone know how to view registers and peripheral (registers)?
The register view is grayed out and the only way that I can presently see where the PC is operating is to use the disassembly view.
Thanks
Regards
Mark
解決済! 解決策の投稿を見る。
Hi Mark,
If views are 'grayed' it means that they are already open. There is no other meaning of this.
So you had them open, but maybe missed the view in the perspective?
I hope this hels,
Erich
Hi Mark,
I don't have a 1020 at hand, so here with the 1051 which is the same for the 1020:
Core registers:
Peripherals+:
which uses a memory rendering:
I hope this helps,
Erich
Eric
Although the register view was grayed out in the Windows -> Show View -> Other-> Debug -> Registers menu I could still click on it and then both the CPU register and Peripherals appeared.
Then I closed the two windows and the Register entry in the menu was no longer grayed out so I could re-enable the register view again normally (but it didn't this time switch in the Peripherals too).
I needed to search to re-enable the peripheral view since it is in Windows -> Show View -> Other->MCUXpresso IDE -> Peripherals+ instead.
But all seems OK now.
Thanks
Mark
Hi Mark,
If views are 'grayed' it means that they are already open. There is no other meaning of this.
So you had them open, but maybe missed the view in the perspective?
I hope this hels,
Erich
Eric
You may be right.
Regards
Mark