RT1060SDK v2.11.0 can not be installed into IDE MCUxpresso V11.3.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1060SDK v2.11.0 can not be installed into IDE MCUxpresso V11.3.0

ソリューションへジャンプ
1,064件の閲覧回数
ZHOU_XIAO
NXP Employee
NXP Employee

Hello , all 

 

My customer wants to use the RT1060 SDK v2.11.0 (Wifi WPS related sample project).

However the SDK v2.11.0 can not be installed into IDE MCUxpresso V11.3.0 like following pictures.

sdk install error.png

 

As an alternative and temporary  solution, I tried to use install IDE MCUxpresso V11.5.0.    As a result , RT1060SDK v2.11.0 can be  installed into IDE MCUxpresso V11.5.0 and works well.

 

Is there other way to fix the install problem (RT1060 SDK 2.11.0 and MCUXpresso 11.3.0) ? or will this problem will be solved in future by some plug-in?

 

 

 

Best regards

ZHOU

0 件の賞賛
1 解決策
1,052件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Hi,

Newer SDK versions are updating functionalities which might not be compatible with previous IDE versions. This is the reason for your error.

Updating to IDE 11.5.0 should not be a temporary solution, but the actual solution.

An workaround (in fact, an expected flow) will be to use an older SDK version with IDE 11.3.0, but our recommendation is to stay on latest IDE with latest SDK versions.

Regards.

MCUXpresso IDE Support

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
1,053件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Hi,

Newer SDK versions are updating functionalities which might not be compatible with previous IDE versions. This is the reason for your error.

Updating to IDE 11.5.0 should not be a temporary solution, but the actual solution.

An workaround (in fact, an expected flow) will be to use an older SDK version with IDE 11.3.0, but our recommendation is to stay on latest IDE with latest SDK versions.

Regards.

MCUXpresso IDE Support

0 件の賞賛
1,036件の閲覧回数
ZHOU_XIAO
NXP Employee
NXP Employee

Thanks for your answer.

0 件の賞賛