MCUXpresso with MKL28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso with MKL28

812 Views
paolocolombo
Contributor III

Hi, I'm starting the development of an application with MKL28. The IDE I am using is Mcuxpresso, last version. I have seen that the "PINS" function is supported, but I have problems with the configuration of the peripherals. I have also seen that the "Peripheral Configuration" menu is not active: the screen says "MCU is not supported". How can I initialize peripherals? Thanks. Paolo Colombo

Tags (1)
0 Kudos
Reply
1 Reply

697 Views
marek-trmac
NXP Employee
NXP Employee

Hi Paolo,

Peripherals Tool was added at the begging of this year (since Config Tools V4.0) and devices and components are being added incrementally. I do not have any information if and when MKL28 will be added.

Regards

Marek

Regards,
Marek
0 Kudos
Reply