LPCXpresso Build Failed due to Auto Generated Files

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso Build Failed due to Auto Generated Files

936 次查看
palak_patel
Contributor II

Hi,

I am using JN-AN-1217 Application note as our base for JN5179 Application Development.

We just created our setup in Linux Environment.

We have installed LPCXpresso v7.9.2 [Build 493] [2015-09-14] .

First I placed this APK in /root/LPCXpresso/workspace. but I couldn't build my project.

   As it was showing no rule to make target.

Then I realized and placed my APK in /usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples.

Here When i perform Clean operation. it works as expected.

But when I build for any one of the configuration ( Coordinator,JN5179,DR1199 ) , It actually starts building the Project but every time it stops at the same point and shows 

19:05:40 **** Build of configuration Coord

19:05:40 **** Build of configuration Coordinator, JN5179, DR1199 for project JN-AN-1217-Zigbee-3-0-Base-Device ****
make JENNIC_CHIP_FAMILY=JN517x JENNIC_CHIP=JN5179 DR=DR1199 GROUPS=0 ICODES=1 APP_NTAG_ICODE=0 APP_NTAG_AES=0 all
Using LPC XPresso toolchain
Using gcc-ar
JENNIC_MAC is Mini MAC shim
JENNIC_MAC_PLATFORM is SOC
Building trace version ...

...

...

...

...

...
/usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples/Zoning_System/Coordinator/Source/zps_gen.c:528:1: warning: initialization makes integer from pointer without a cast
 PRIVATE ZPS_tsAplApsmeBindingTable s_bindingTable = { 0, s_bindingTableStorage, 4 };
 ^
/usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples/Zoning_System/Coordinator/Source/zps_gen.c:528:1: warning: (near initialization for 's_bindingTable.u32SizeOfBindingTable')
/usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples/Zoning_System/Coordinator/Source/zps_gen.c:528:1: warning: excess elements in struct initializer
/usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples/Zoning_System/Coordinator/Source/zps_gen.c:528:1: warning: (near initialization for 's_bindingTable')
/usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples/Zoning_System/Coordinator/Source/zps_gen.c:552:5: warning: large integer implicitly truncated to unsigned type [-Woverflow]
     0x00000800UL,
     ^
Makefile:385: recipe for target '/usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples/Zoning_System/Coordinator/Build/zps_gen.o' failed
/usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples/Zoning_System/Coordinator/Source/zps_gen.c:567:5: warning: large integer implicitly truncated to unsigned type [-Woverflow]
     0x1770,
     ^
/usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples/Zoning_System/Coordinator/Source/zps_gen.c:568:5: warning: initialization makes integer from pointer without a cast
     au32IncomingFrameCounter,
     ^
/usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples/Zoning_System/Coordinator/Source/zps_gen.c:568:5: warning: (near initialization for 's_sAplAib.u16ApsSecurityTimeOutPeriod')
/usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples/Zoning_System/Coordinator/Source/zps_gen.c:568:5: error: initializer element is not computable at load time
/usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples/Zoning_System/Coordinator/Source/zps_gen.c:568:5: error: (near initialization for 's_sAplAib.u16ApsSecurityTimeOutPeriod')
make: *** [/usr/local/lpcxpresso_7.9.2_493/lpcxpresso/Examples/Zoning_System/Coordinator/Build/zps_gen.o] Error 1

19:05:41 Build Finished (took 1s.266ms)

I can not understand where is the Problem actually.

Please help.

标签 (1)
0 项奖励
3 回复数

771 次查看
shreel_chhatbar
Contributor I

Hey Mario,

I am also facing the similar issue , Can you let me know what exactly does it mean by "not supported"?

Is it not support for Linux Platform?

0 项奖励

771 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Shreel,

The LPCxpresso is support for Linux Platform.

Regards,

Mario

0 项奖励

771 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Johan,

As you know, the JN5179 is not supported. Could you please get in contact with your NXP Sales?

Regards,

Mario

0 项奖励