Hi,
I am working on FRDM tower boards to establish CAN bus communication. I was successful in my approach to send and receive data between two FRDM tower boards using CAN bus. However, I am not able to understand few parts.
1. What is a mailbox? Is this the CAN ID for the device or this specifies the memory location?
2. In flexcan_interrupt_transfer.c example,
/* Set Rx Masking mechanism. */
FLEXCAN_SetRxMbGlobalMask(EXAMPLE_CAN, FLEXCAN_RX_MB_STD_MASK(rxIdentifier, 0, 0));
is used. Why does there have to be a masking?
Now I am trying a receive data from a different board into my tower board using CAN bus. But the other board does not have flexCAN, it works like a simple CAN. My other board is sending its CAN ID, Node ID and data altogether where I need to mask it in tower board side to get individual ID.
I am not able to get a clear idea of how FlexCAN works.I checked but could not find any documentation which would explain me the basics of flexcan. It would be great if someone could point me in the right direction in above questions and documentation as well.
Board: twrKf120
Example: flexcan_interrupt_transfer
Thank you
Thanks and Regards
Niranjan
已解决! 转到解答。
Hi Niranjan,
Please check the following link:
https://www.nxp.com/docs/en/reference-manual/K21P144M120SF5RM.pdf
I was wrong , the chapter is the 48, I will put the chapters corrected bellow.
1.- Please check the section 48.4, there there explain the structure of the mailbox.
2.- Please check the section 48.3.5, this is the register write in this function.
Also, for your second question check the section.
48.3.35 Rx FIFO structure
I think the RTR bit should help you to do what you want.
Best Regards,
Alexis Andalon
Hi Niranjan,
1.- Please check the section 52.4, there explain the structure of the mailbox.
2.- Please check the section 52.3.5, this is the register write in this function.
3.- FlexCAN works the same as CAN, only include some extra functionality.
As a suggestion, first I will try the loopback example and after that try connecting with the other board.
Best Regards,
Alexis Andalon
Hi,
adding one more question to below one:
FlexCan has a global Mask function (SetRxMbGlobalMask) but I wanted to use filter function as well. I could not see a default function like that? Can you tell me whether I have to write up a particular function to filter out the IDs or any workaround is possible in existing functions?
The id which I am looking to filter out is 0x760. I am not bothered about the rest of the IDs from the other device.
Thank you
Thanks and Regards
Niranjan
Hi Niranjan,
Please check the following link:
https://www.nxp.com/docs/en/reference-manual/K21P144M120SF5RM.pdf
I was wrong , the chapter is the 48, I will put the chapters corrected bellow.
1.- Please check the section 48.4, there there explain the structure of the mailbox.
2.- Please check the section 48.3.5, this is the register write in this function.
Also, for your second question check the section.
48.3.35 Rx FIFO structure
I think the RTR bit should help you to do what you want.
Best Regards,
Alexis Andalon
Hi,
Thank you for your inputs. I was able to get a partial code get working.
Now I am facing issue in the TxIdentifier [mailbox] . The frame holds id and data in flexcan. The destination CAN ID to which I had to send the data is 1002F801(Hex value).
So I mapped 1002F801(Hex value) to my frame.id parameter(like frame.id = 0x1002F801 ) in flexcan code , its not sending the frame like how i expect.
I used an external SLCAN adapter to visualize it . I could see the CAN ID as 178 and 05 C9 is my value which i am sending.
I checked MCU xpresso code and I could find this
Few puzzling things are:
1.frame.id = 0x1002F801 is good enough to map the destination frame id? Or any work around is needed over here? Not sure how.
2. With respect to Tx, does TxIdentifier can be different from frame id? Because in the example code I could see frame.id being derived from TxIdentifer(29 bit identifier mask) [I also have a 29 bit identifier in my case in both sides].
Whereas, I know the destination id [1002F801] to which I need to send the data. Any simple approach is possible?
Any pointers would be helpful.
Thank you
Thanks and Regadrs
Niranjan