Demo evkbmimxrt1170_rpmsg_lite_pingpong does not work.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Demo evkbmimxrt1170_rpmsg_lite_pingpong does not work.

跳至解决方案
806 次查看
simmania
Contributor III

I have the MIMXRT1170-EVK board. I installed the SDK_2.x_MIMXRT1170-EVKB. And imported the demo. The demo consists of the two subprojects:
evkbmimxrt1170_rpmsg_lite_pingpong_cm4
evkbmimxrt1170_rpmsg_lite_pingpong_cm7

I can compile it without errors. But when running (the cm7) I get the following error:

simmania_0-1686601161723.png

What am I doing wrong?

 

0 项奖励
回复
1 解答
757 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @simmania ,

No, he is wrong. EVKB and EVK are different board although very similar. 

Please download sdk from https://mcuxpresso.nxp.com/en/welcome

 

Regards,

Jing

在原帖中查看解决方案

0 项奖励
回复
4 回复数
743 次查看
simmania
Contributor III

I created the SDK with SDK Builder and selected the evkmimxrt1170 board in stead of the evkbmimxrt1170 board. Now the demo works! Thanks.

0 项奖励
回复
779 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @simmania ,

I tested on my EVK with SDK_2_13_0_MIMXRT1170-EVK. It works fine. Please don't use EVKB SDK. Sometimes a slight difference will cause the demo can't run. 

Please also check if you have switch the board to serial download mode and erase the flash before debug.

 

Regards,

Jing

0 项奖励
回复
772 次查看
simmania
Contributor III

This confuses me.

Firstly because an other NXP Techsupport told me to use the B version.
See https://community.nxp.com/t5/MCUXpresso-IDE/What-is-difference-between-evkmimxrt1170-and-evkbmimxrt1...

Secondly because the demo is part of the SDK, isn't it?

So the SDK_2.x_MIMXRT1170-EVK has its own demos and SDK_2.x_MIMXRT1170-EVKB also has its own demos.

I also found out that the evkbmemxrt1170_iled_blinky_cm4 does work, but the evkbmemxrt1170_iled_blinky_cm7 does not.

 

0 项奖励
回复
758 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @simmania ,

No, he is wrong. EVKB and EVK are different board although very similar. 

Please download sdk from https://mcuxpresso.nxp.com/en/welcome

 

Regards,

Jing

0 项奖励
回复