Debian package of MCUXpresso IDE requires udev

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debian package of MCUXpresso IDE requires udev

370件の閲覧回数
stefanct
Contributor III

mcuxpressoide-11.9.0_2144.x86_64.deb executes `udevadm` as part of its `postinst` script. This command is installed with the `udev` pacakges, which might not be the case... such as with the default Docker image of Debian 12 because it simply does not make any sense there really.

I would prefer the compiler to be shipped individually without such shenanigans instead of together with Eclipse anyway. However, if the package actually requires it, it should depend on it, which it currently does not.

タグ(1)
0 件の賞賛
返信
1 返信

355件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @stefanct,

Thanks for reporting this. I will deliberate about this topic with internal to see what changes can be made or how to optimize the unnecessary packages.

BR,
Edwin.

0 件の賞賛
返信