Configuring a new MCUXpresso Project driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring a new MCUXpresso Project driver

1,635件の閲覧回数
anbui
Contributor II

Why are the drivers I select when setting up my project not pulled and put in the project?

Do I need to copy each one individually over?

or

Am I selecting a wrong option?

0 件の賞賛
返信
1 返信

1,530件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

When you click on the new project wizard's Finish button, all of the selected driver files should be copied into the project created in your workspace. There will be a number of folders created within the project, so make sure you check them all to see the driver files.

If you are still having problems, can you provide more details of what the project you create actually contains?

Note : For more details of creating projects, please check out the MCUXpresso IDE User Guide, supplied as part of the product install.

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信