Hi all,
I'm using the (last) MCUXpresso IDE v11.2.1 [Build 4149] [2020-10-07].
I can't Exclude from build a folder that I added to a project.
I used to do it without a problem on a previous IDE version. I'd like to avoid to reinstall also another older version (I've just got a clean installation) to check this.
am I the only one got this issue or is it a bug? I attach screenshots of the matter.
excludeBuild_01 -> see all folders icon before the operation;
excludeBuild_02 ->execution of the command on both the configurations;
excludeBuild_03 ->result after command run. All folders look still considered for the build.
Best regards,
AGA
解決済! 解決策の投稿を見る。
To be included in a build, the folder needs to be a source folder. If it is not a source folder, it is automatically excluded from the build.
From your '01 screenshot, there are no source folders, so excluding does not make sense.
Hello AGA,
Thanks for your sharing.
Regards,
Alice
Your parent/root folder needs to be *included* into the build and should have a 'S' as Icon decorator to indicate it contains sources.
Hi @ErichStyger,
Yes that solves the issue.
For sure my mind failed to remember the steps I made..
Thank you very much!
AGA
To be included in a build, the folder needs to be a source folder. If it is not a source folder, it is automatically excluded from the build.
From your '01 screenshot, there are no source folders, so excluding does not make sense.