MCUXpresso IDE v11.9.1 Now Available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE v11.9.1 Now Available

MCUXpresso IDE v11.9.1 Now Available

We are pleased to announce that MCUXpresso IDE v11.9.1 (build 2170) is now available. 

This is a maintenance release that builds upon the previous MCUXpresso IDE v11.9.0 release and we recommend that all existing users download and install this new version.

 

Installer Downloads 

To download the installers for all platforms, please login to our download site via: 

 

Documentation 

Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built-in help system available via IDE's Help menu and in PDF form from within the installation directory.

 

Notification of future releases 

To receive notifications about future releases, please follow: MCUXpresso IDE - Release History 

 

Summary of Changes - version 11.9.1 - April 2024

  • Upgraded: Newer LinkServer software (v1.5.30)
  • Upgraded: Newer SEGGER J-Link software (v7.96c).
  • Upgraded: Newer PEmicro plugins (v5.7.8).
  • Updated: Version v15.1 of MCUXpresso Config Tools.
  • Improvement: [IDE] Updated licensing text from the About window.
  • Improvement: [IDE] Support Eclipse variables for J-Link script file inside launch configuration.
  • Fixed: [IDE][SDK Handling] Automatic import of plugin SDKs returns an error if the IDE isn't installed in the default location.
  • Fixed: [IDE][SDK Handling] Automatic import of plugin SDKs fails to import some SDKs.
  • Fixed: [IDE][Config Tools Integration] Fix some performance issues.
  • Fixed: [IDE][Welcome page] Release notes text shown in What's New section might be incorrectly rendered.
  • Fixed: [KW45/K32W1][J-Link] Debug after flash erase does not work.

 

Known issues 

  • Please follow the KnownIssues.txt file from installation layout for a detailed list.
No ratings
Version history
Last update:
a week ago
Updated by: