V11.0.0 SWO Data not working for 55s69

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

V11.0.0 SWO Data not working for 55s69

673件の閲覧回数
AndyCapon
Contributor II

Hi Guys,

First thanks for adding SWO stuff in for this board.

Unfortunately for me the data watch is not working.

While paused in the debugger I can add a global variable and the Value is displayed correctly.

Then when execution is resumed to value is displayed as 0 and no events are recorded.

It is easy to replicate, start by importing the hello_world_swo example.

Add a global unsigned int count variable, and increment this in the run loop.

Add a breakpoint in the loop and start debugging.

Now add a BWT item for the count variable, you will see it has the correct value.

Remove breakpoint and resume execution, values goes to 0 and stays there.

Any ideas ?

Thanks

Andy

pastedImage_1.png

unsigned int  uCount = 0;
int main(void)
{
    /* Init board hardware. */
    /* attach 12 MHz clock to FLEXCOMM0 (debug console) */
    CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);
    /*!< Switch TRACE to TRACE_DIV */
    CLOCK_AttachClk(kTRACE_DIV_to_TRACE);

    BOARD_InitPins();
    BOARD_BootClockFRO12M();
    BOARD_InitDebugConsole();
    BOARD_InitKey();
    BOARD_InitDebugConsoleSWO(DEMO_DEBUG_CONSOLE_SWO_PORT, DEMO_DEBUG_CONSOLE_SWO_BAUDRATE);
    while (1)
    {
      uCount++;
       if (g_userPress)
       {
         PRINTF("SWO: hello_world\r\n");
         g_userPress = false;
       }
    }
}
0 件の賞賛
2 返答(返信)

564件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Andrew,

 

Thanks for your feedback! I will report this internally so we can fix this issue in future releases.

 

Best regards,

Felipe

0 件の賞賛

564件の閲覧回数
AndyCapon
Contributor II

Thanks Felipe.

0 件の賞賛