SPI communication with PCF2123

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI communication with PCF2123

499 次查看
louis_eeckeloot
Contributor I

Hi,

I would like to communicate with SPI between my microcontroller (PN7462) and my RTC : PCF2123.

I don't know how to proceed, how to program it on MCUXpressoIDE.

Is someone have a code example for my request ? with the code lines I have to write in my code.

Thanks,

BR,

Louis.

标记 (1)
0 项奖励
回复
1 回复

431 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Louis,

Unfortunately there isn't any example for the RTC using this MCU, you will need to start from the SDK that is available in the following link:

NFC Reader Library | NXP 

After download the library, in MCUXpresso select the option Import project(s) from file system:

pastedImage_6.png

Look for the route where you install the sofware, and select in the PN7462AU Software the zip file.

pastedImage_4.png

After that, click the finish button.

In the folders that were imported to your workspace, in the following route you'll find the SPI driver need it to communicate with the RTC: PN7462AU->phHAL->phhalSPIM

In this driver you will find all the functions to communicate through SPI with the RTC.

Also in the following link, in the chapter 12,  you can find the sequence of initialization for this RTC, it use I2C to explain but the commands are the same: https://www.nxp.com/docs/en/user-guide/UM10301.pdf  

Let me know if this helps you.

Best Regards,

Alexis Andalon

0 项奖励
回复