RT1050 OTA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050 OTA

822 Views
jonver
Contributor II

Is there support for an OTA update of the RT1050? 

I suppose it would take the following steps: (correct me if i'm wrong)

- load flashloader application into RAM from the main application (not the rom bootloader)

- rewrite the flashloader so it communicates via our own communication channel instead of the USB

Can the flashloader be loaded into ram without using the rom bootloader?

Thanks!

Labels (1)
0 Kudos
1 Reply

619 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Jonathan Vervaeke

RT1050 has a secondary bootloader (MCUBoot), it is included in the SDK MCUXpresso as middleware, and you can use this flashloader to work with the serial communication, you will only need to follow the protocol of the MCUBOOT.

Best regards

Jorge Alcala

0 Kudos