I'm running the latest MCUXpresso IDE (v10.2.0). I have built and installed current v2.4 SDK's for MKL17Z processors from the MCUXpresso SDK builder site.
I'm trying to create a new project using the SDK Builder wizard, but when I get to the step where you select which drivers and middleware to include, the list of drivers is completely empty except for the clock driver.
I'm sure I haven't had this issue before using older IDE/SDK versions, and the problem doesn't occur if I use a different processor from a similar family (eg KL16Z, KL27Z), or different processors entirely (eg KL28Z, K64F).
Is this just a bug with the IDE and/or SDK, or is the KL17Z no longer supported ?
HI geoff_s
Please download the latest SDK 2.4 packages from NXP website again. The old versions seems have problems. Now it has been fixed.
Regards
Daniel
Hi,
I'm still missing the driver and also examples for DAC.
Regards
Hi Norbert Witt
There are two chips for KL27, only one has 12-bit DAC.
For frdmkl27 board, no dac component.
If your chip has 12-bit DAC, you can use the DAC driver in KL43.
Regards
Daniel