No compatible probes available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

No compatible probes available

455 次查看
nxp9
Contributor I

I have a FRDM-KE02Z40M board.  It uses OpenSDA V1.  I have not been able to find any way to download the board, either release or debug, without coming up against this error message.  I am under Windows 10.  The USB port is shown as working OK in the device manager, and the Explorer view of the board is as described in the OPENSDAUG.pdf documentation.

What do I have to do to download this board?

标签 (1)
标记 (1)
0 项奖励
1 回复

349 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

As we talked in the case:

Please download the latest OpenSDA Firmware (MSD & Debug)

OpenSDA Firmware (MSD & Debug).png

You need to following the steps descripted in BOOTUPDATEAPP_release_notes.txt and using BOOTUPDATEAPP_Pemicro_v111.SDA update the bootloader to 1.11.
After update the bootloader to 1.11, he need to update the firmware to 1.18 using MSD-DEBUG-FRDM-KE02Z_Pemicro_v118.SDA.

update bootloader.png

notice: Please using Win7 PC

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励