No compatible probes available.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No compatible probes available.

1,027 Views
running_gao
Contributor I

Hello NXP,

 

I downloaded the new MCUXpresso IDE_11.2.1_4149. I can build a project but when I click on 'Debug', I get an error message – “No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target”. The board is powered up and I am using Ubuntu V16+. Please advise. 

0 Kudos
1 Reply

1,023 Views
ErichStyger
Senior Contributor V

Hi @running_gao ,

do you have a probe/board connected? Using the correct USB port (some boards only do have a debug probe on some USB ports).

You should see the debug probe in your device list too.

 

I hope this helps,

Erich

0 Kudos