Hi,
I have FRDM-K22F Board, and I try to light the RGB Led on the board. According to the user guide <FRDMK22FUG.pdf>, the Red color controlled by pin PTA1, the Green controlled by Pin PTA2. On the MCU datasheet <K22F Sub-Family Reference Manual> page1359, address 400F_F014 is port data direction register, address 400F_F000 is port Data Output Register.
I use MCUXpresso IDE to import example <frdmk22f_hello_world, and add codes as below:
PRINTF("hello world.\r\n");
*(int*)0x400FF014 = 0x02; //set PTA1 as Output – my code
*(int*)0x400FF000 = 0x02; //set PTA1 as High, so the led should be red -my code
while (1)
{
ch = GETCHAR();
PUTCHAR(ch);
}
There is no error to “Build” and “Debug”, but the RGB Led always keep green.
Appreciate for any help on this.
解決済! 解決策の投稿を見る。
Hello Tony Tao ,
Please set PTA1 to low , then the RED LED should be on .
Have a look at the schematic of FRDM-K22 board :
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Alice,
Appreciate your reply, I was using Kinetis Design Studio 3 IDE and Processor Expert, and be advised to use MCUXpresso.
I was expect the MCUXpresso and config tool should is as easy as Processor Expert.
and on the Processor Expert, there is a way to W/R register directly. that is why the question come from.
but thank you again for your time, it help a lot.
have a good day!
Hello Tony,
You are welcome .
In MCUXpresso IDE, you can also use Pins Tool, Clocks Tool and Peripherals Tool to configure
like Processor Expert, about detail please take a look at "MCUXpresso_IDE_User_Guide.pdf"
->12. MCUXpresso Config Tools .
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
*(int*)0x400FF014 = 0x06; //set PTA1 (Red) & PTA2 (Green) as Output
*(int*)0x400FF0D4 = 0x20; //Set PTD5 (Blue) as Output
*(int*)0x400FF000 = 0x06; //set PTA1 & PTA2 as High
*(int*)0x400FF0C0 = 0x20; //set PTD5 as High
that is the code I wrote. I set all PTA1, PTA2, PTD5 to High, and the RGB LED should be OFF, but the LED just keep Green.
and I tried different setting (like set PTA1 as low), but it look like the code did nothing on it, just the LED keep green. Did I do something wrong else?
Hello Tony,
Firtly, please enable the clock of PORTA and PORTD,
then config PTA1 PTA2 and PTD5 to as GPIO :
CLOCK_EnableClock(kCLOCK_PortA);
CLOCK_EnableClock(kCLOCK_PortD);
PORT_SetPinMux(PORTA, 1U, kPORT_MuxAsGpio);
PORT_SetPinMux(PORTA, 2U, kPORT_MuxAsGpio);
PORT_SetPinMux(PORTD, 5U, kPORT_MuxAsGpio);
*(int*)0x400FF014 = 0x06; //set PTA1 (Red) & PTA2 (Green) as Output *(int*)0x400FF0D4 = 0x20; //Set PTD5 (Blue) as Output
*(int*)0x400FF000 = 0x06; //set PTA1 & PTA2 as High
*(int*)0x400FF0C0 = 0x20; //set PTD5 as High
Hope it help,
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Alice,
thank you so much for you replay!
But I still have two problem:
1. when I add the code above and try to build the code , I got an Error of 'kPORT_MuxAsGpio' undeclared (first use in this function) and the building stop at :
PORT_SetPinMux(PORTA, 1U, kPORT_MuxAsGpio);
when I try to open the pins icon,
the IDE tell me No processor selected, but on the Project Settings - MCU, the setting is MK22FN512VLH12 already.
2. could you please tell me what is GPIO clock, why I have to Enable it? and what does "PORT_SetPinMux(PORTA, 1U, kPORT_MuxAsGpio);" doing?
Hello Tony,
1. The definition of "kPORT_MuxAsGpio" is in fsl_port.h file , please include it :
#include "fsl_port.h"
2. Before we use the port , we need to first enable the clock , please have a look at the Reference Manule of your chip :
3. I was wondering why you configure registers by yourself on by one , you can use SDK driver to configure,
also there is gpio demo under SDK package :
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Tony Tao ,
Please set PTA1 to low , then the RED LED should be on .
Have a look at the schematic of FRDM-K22 board :
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------