MCUXpresso IDE high CPU usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE high CPU usage

1,244 Views
nxa09603
NXP Employee
NXP Employee

Hi

MCUXpresso IDE demands almost 30% usage of my CPU in idle. During debug process, it gets up 80%. It that normal? I have an i7 Dell Ultrabook with SSD + 8G RAM.

@Thank you

Andre VB

Tags (1)
0 Kudos
3 Replies

1,022 Views
ErichStyger
Senior Contributor V

No, that's certainly not normal.

this is what I have while debugging a Kinetis on Windows 10 with V11.0.1 using J-Link:

pastedImage_4.png

So it really does not add up. Are you using the V11.0.1 (NXP MCUXpresso IDE 11.0.1 available | MCU on Eclipse ) too?

I know that this might be somewhat different between debug probes (P&E, SEGGER, LPC-Link), but in general it is not above 5% or so.

I hope this helps,

Erich

0 Kudos

1,022 Views
nxa09603
NXP Employee
NXP Employee

Hi Erich

Latest MCUXpresso version(V11.0.1). Board is the FRM-KL25, P&E probe. I have been noticed the same behavior in desktop PC as well.

Maybe not related but the tool looks heavy, specially if I use Semihost. With Semihost I have to restart the application every time when I lunch compilation. I stop using it and it and the tool gets faster, less restart, but still high CPU usage.

Thanks

AndreVB

0 Kudos

1,022 Views
ErichStyger
Senior Contributor V

Ok, I see a 20% CPU load with using P&E for the FRDM-KL25Z. I'll get in touch with P&E about this...

Erich

0 Kudos