MCUXpresso IDE and Kinetis devices

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso IDE and Kinetis devices

1,741 次查看
rodrigocavalcan
Contributor I

Hi,

   I'm starting the work with MKM34z and I'm switching to use the MCUXpresso for it. I already use the MCUXpresso for LPC devices. I cannot find any Kinetis family device on the list when I try to create the project. I already re-installed the IDE and switched to a new workspace. When I try to use the MCUXpresso Config Tools, I can see only a subset of Kinetis devices. On this list I can see the MKM34256xxx7, but not other variant with the 100 pins.

   Now I don't know if I'm supposed to use the new MCUXpresso, if it have support for these parts, or if I have to continue using the KDS IDE.

   Please enlighten me,

   Thanks,

   - Rodrigo

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,076 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Rodrigo.

So far, MCUXpresso only supports parts of kinetis project.

here is MCUXpresso Supported Devices Table for reference

MCUXpresso Supported Devices Table 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复