first a friendly Hello to the support engineers :
mcuxpresso 10.0.2 (411) fresh install on win 10 pro 1703 on dell e6430 laptop
my own lpc824 project compiles, but doesn't load : "no compatible probes available"
the lpc824-max mbed device shows up as "mbed cmsis-dap" in control panel devices and printers
why does mcuxpresso not see the probe for / in it
i also attached a few pics to show some of the below mentioned results ... any reference to win10_pro_1703 refers to the computer where i experience this problem and win10_home_1607 refers to the working win computer
the win 10 pro 1703 has a brand new windows install to get started with and no previous left overs from upgrades ... also the 1607 and 1703 refers to the win 10 rev levels ... i was not able to upgrade the working win 10 home from 1607 to 1703 ... some windows upgrade issues ... win10_home_1607 is an hp 17e189 ... both have 16 gb ram
for comparison :
my lpc54114 project compiles and loads (runs) on the same win 10 pro 1703 laptop without any problems
my lpc824 project compiles and loads (runs) on all linux (kubuntu 1604) boxes
my lpc824 project compiles and loads (runs) on other win 10 home 1607, which was upgraded from win 8.1 and had previous lpcxpresso versions installed
i also tried it with lpcxpresso 822.2.650 and a brand new empty lpcopen C++ project ... it compiles but doesn't load
maybe this is an issue for you Brandon or Steve, cheers Klaus
Hi Klaus,
You may be interested to know that we recently released a new set of debug firmware and Windows 7 drivers for our boards that feature the LPC11U3x MCU as a debug probe (so all the "MAX" boards). The new firmware can be found under the Software & Tools tab of the board page (so for you the URL to the board is http://www.nxp.com/demoboard/om13071).
The intention is for this firmware to be used instead of the mbed-based firmware and driver that has been used up until now, if you are not going to use Mbed (you can continue to use the Mbed version if you so wish however). Some reasons to consider the new firmware & driver:
I'm going to post a blog note about this now.
Best regards,
Brendon
one more thought would be ... how is it possible that the lpc54114 works on this computer and the mbed 824 device NOT ???
also could there be a clue in how the mbed device shows up in control panel devices and printers ... as example
working : MBED microcontroller USB Device
failure : MBED CMSIS-DAP
why is the display appearance different ... is it the different windows version "pro 1703" vs "home_1607" or is the mbed driver for it different
i would also like to mention my usb connection ... i tried it with several usb cables on at least 2 usb ports if not all 3 (don't remember)
what i know for sure is that all the tests, where the screen-shot pics have been taken, were done with a sabrent 4 port usb 3 hub and also with a sabrent 4 port usb2 hub, where the board was connected to ... the hub was plugged into i believe, was a usb 2 port
maybe this info helps to narrow it down or for reproduction purpose
thanks and cheers Klaus
Hi Klaus,
Could you try softloading the debug probe firmware into the board, If the DFULink is fitted on the board, then the IDE should softload the firmware. I would also suggest that you try booting the probe (i.e. soft loading the firmware) manually. Information on how to do this is described in the MCUXpresso IDE User Guide - section 14.12.4, " Manually booting LPC-Link2". You could also review the troubleshooting section in 14.12.7, and see if the suggestions work.
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer
first of all, thanks Carlos and sorry that it took a while to respond
i didn't really understand too much with regards to " Manually booting LPC-Link2" and tried something else which seemed easier to me and for now it worked
the link below showed a similar problem and i took a closer look and followed one advise in it
LPCXpresso 824 Max error "no compatible emulators"
it suggested :
And have you installed the mbed serial port driver, or are you relying on the Windows 10 built in driver? Windows serial configuration - Handbook | mbed
and i followed it to the mbed "windows serial link configuration" (link above) and installed as instructed
and this made it work ... beautiful :smileywink:
now the lpc824max shows up in control panel -> devices and printers as "MBED microcontroller" like on the win10_home_1607 where it worked, and no longer as simple "MBED CMSIS-DAP" device
this all would make a bit sense, since this win 10 schlepptop had a virgin win_10_pro_1703 and everything else newly installed, as compared to the other win10_home_1607 where i used it for the past 3 years-plus for a lot of lpc... development work ... and i must have back then installed this mbed driver ... maybe even during the glorious win 8.1 days or it came with an earlier lpcxpresso version
let's hope this was it
thanks again Carlos