How to optimize the ADC Section only?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to optimize the ADC Section only?

569件の閲覧回数
chennai2chn
Contributor I

Optimize -O1 using External-ADC working is fine but other interfaces is too bad performance.... how to apply

specific section optimize.... Kinetis Series processor used...

Advance Thanks

ラベル(1)
タグ(1)
0 件の賞賛
1 返信

524件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check below thread about the question:

https://community.nxp.com/thread/28716

Please check the ADC module registers value difference after code initialization with/without optimize enabled.

Thanks for the attention.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛