Hi,
I am not sure if I understand your questions.
To work with KL16Z64, if using MCUXpresso, we need install
1. MCUXpresso IDE
2. MCUXpresso SDK
https://mcuxpresso.nxp.com/en/welcome
After you install SDK, you will see there are many SDK examples under the install folder. If you are beginner, One suggestion for you is, you find an example that is closest to your project requirement, import this example to IDE. you can revise it and add your own code based on it.
Besides, here is some training videos
If anything is still not clear, please let me know the specific.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HELLO:
My IDE is IAR.
Thank you .
--
牛志刚
主页:Http://www.mnshanghai.com <http://www.mnshanghai.com/>
电话:021-35303166
手机:13817023673
If you use IAR, you can also use SDK with it. download SDK for IAR version.
after you install it, you will see IAR demo code inside the folder.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
应该是生成,不是生产