mex_configuration_1.9.xsd NOT FOUND

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mex_configuration_1.9.xsd NOT FOUND

Jump to solution
2,494 Views
MichaelV
Senior Contributor II

Hi,

The xsd for the latest Config Tools for iMX is again not available on http://mcuxpresso.nxp.com/XSD/mex_configuration_1.9.xsd. It was the same with the 1.8 version (it was fixed some time after we notified NXP support of the problem). We need the xsd to process mex files using our internal tool. Can you please make this file available?

Thanks.

0 Kudos
Reply
1 Solution
2,470 Views
liborukropec
NXP Employee
NXP Employee

Hi Michael,

 

thank you for reporting this issue. It has been fixed now.

 

Regards,

Libor

View solution in original post

4 Replies
2,471 Views
liborukropec
NXP Employee
NXP Employee

Hi Michael,

 

thank you for reporting this issue. It has been fixed now.

 

Regards,

Libor

1,564 Views
MichaelV
Senior Contributor II

Hi,

The same is true for every version released after 1.9:

https://mcuxpresso.nxp.com/XSD/mex_configuration_1.10.xsd

https://mcuxpresso.nxp.com/XSD/mex_configuration_1.11.xsd

https://mcuxpresso.nxp.com/XSD/mex_configuration_1.12.xsd

https://mcuxpresso.nxp.com/XSD/mex_configuration_1.13.xsd

None are available. Can you please add to the team's instructions to upload the xsd file to the mcuexpresso server whenever they release a new version of the Config Tool?

For now, please make sure all the above files are available. Thanks!

0 Kudos
Reply
1,546 Views
Petr_H
NXP Employee
NXP Employee

Hi,

The new XSDs are available, but there has been a change in the name of XSD file after the V9 so the URLs that you anticipated will not work. You need to use the following URLs:

https://mcuxpresso.nxp.com/XSD/mex_configuration_10.xsd

https://mcuxpresso.nxp.com/XSD/mex_configuration_11.xsd

https://mcuxpresso.nxp.com/XSD/mex_configuration_12.xsd

https://mcuxpresso.nxp.com/XSD/mex_configuration_13.xsd

best regards

Petr Hradsky

Config Tools Team

1,544 Views
MichaelV
Senior Contributor II

Great, thank you!

0 Kudos
Reply