SPC5668G can't run software and can't erase flash,why?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPC5668G can't run software and can't erase flash,why?

1,046 Views
ypchang
Contributor II

When the controller was running , I touch the power chips to know the heating,  then SPC5668G suddenly not run . Later I find the flash can’t be erased by BDM and IC5000. The software can’t be download.    How can I do next? 

0 Kudos
2 Replies

749 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please write me, if you use LQFP or BGA package? Also I need to know, if you have soldered the microcontroller or if you use socket.

It is also possible that you destroyed the microcontroller using static charge. At first, please measure reset line and in case reset line is always 0, microcontroller is destroyed. It is also possible that only some part of microcontroller is damaged and this could be the reason you are not able to connect.

Regards,

Martin

0 Kudos

749 Views
marek-trmac
NXP Employee
NXP Employee

Hi Yp Chang,

 

MCUXpresso Config Tools supports Cortex-M Kinetis and LPC devices. MPC devices are not supported.

 

I'd recommend to submit this question to MPC related comunity: https://community.nxp.com/community/s32/mpc5xxx

 

Regards

Marek

Regards,
Marek
0 Kudos