MCUXpresso Config Tools v14.0 Now Available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso Config Tools v14.0 Now Available

MCUXpresso Config Tools v14.0 Now Available

We are pleased to announce that MCUXpresso Config Tools v14.0 are now available.

Downloads

Release Notes

Full details on the release (features, known issues...)

Config Tools v14.0

  • The product is based on Eclipse 2022-12
  • Open JDK 17 is updated.
  • Batch processing on command line is supported.
  • Support for SDK 2.14 in Project cloner and Detect toolchain project is added.
  • Link to a toolchain project on a location different than .mex file is added.
  • The command for discarding changes and reloading .mex (MCUXpresso IDE) is added.
  • Quick fix for errors allows setting the "Called by the default initialization function" flag when it would fix an error.
  • Search functionality to Code Preview is added.
  • TEE
    • MCXN-947 combination of AHBSC with TRDC (MBC) is supported.
    • Export TEE registers via wizard or command line is available.
    • Boot ROM hiding feature is supported.
    • Tier mode for TRDC is supported.
    • Domain ambivalence for RDC masters is added.
    • Master-specific memory alias
    • Validation for A28 bit of MPU region address is added.
    • Memory map filters are aligned with Arm terminology.
    • Status bar is united with other tools.
  • PLU
    • Tools used for Verilog synthesis and model optimization are replaced.
    • Linux, Mac, and Apple silicon platforms are supported.
    • Newer versions of Verilog standard are supported.
    • Creation of flip-flop circuits outside Direct mode is supported.
    • Support for special comment that contains mapping information is added.
    • Support for Verilog code resynthesis is added in the new command-line option.
    • Buttons in Schematic view are reordered to groups of related buttons on each row.
    • Information from Verilog synthesis and model optimization tools is added to the error dialog.
  • Peripherals
    • Migration of Peripherals tool components to the latest supported version on current MCU in command line is supported.
    • User information on the dependency of the tool on another tool disabled in the configuration is improved.
    • Migration report generation is supported.
    • The generated report may contain instructions on how to handle incompatible changes between versions of the configured SDK component.
    • Opening links to websites in the Documentation view in an external browser is supported.
  • Pins
    • Labels defined for Expansion header pins can be set as identifiers of the routed pin.
    • Expansion headers can be locked for editing.
    • Expansion headers and boards are added to the HTML and CSV reports.
    • Columns from Routing Details can be added to the External User Signals view.
    • New External User Signals can be created for all routed pins that are missing in the signals table.
  • Clocks
    • Support for the same frequencies settings from different source for internal clocks is added.

Community

MCUXpresso Config Tools

无评分
版本历史
最后更新:
‎09-12-2023 04:03 AM
更新人: