A new version of the Kinetis Expert Configuration Tools has been released and is available both online (Welcome to Kinetis Expert | Kinetis Expert ) or for download as desktop tool (Software Development Kit for Kinetis MCUs|NXP ).
The set of the tools has a new member: the Clocks Tool:
Main features of Pins Tool and Clocks Tool:
What's New
The release notes of the desktop application are attached to this article.
Clocks Tool
The new member of the suite of configuration tools is the Clocks Tool. Use the Tools menu to select and switch between the tools:
The Clocks Tool provides graphical views for configuration and navigation in the clocks of the hardware:
Templates, Kits, Boards and Processors
When creating a new configuration, it offers Templates, Kits, Boards and Processors.
Custom configurations can be stored as templates and then used for new configurations.
Board Specific Functions
With the provided board and kit configurations, there are now pre-configured initialization functions for major blocks on the board:
Labels and Identifiers
In the Pins Tool there are two new columns: Label and Identifier:
The Label is a user name/string to identify or describe the pin. The Identifier is a user C/C++ identifier which is added to the generated source code to be used by the application.
Export Data
To simplify downloading the device specific data for the desktop tool, the 'Export' function can be used to download and export the data. The data can be copied that way to another machine or all data for a set of devices can be loaded.
The device support for the clocks tool is staged, so initially not all SDK V2 devices are included. As of Oct 14, the the following Kinetis SDK V2 R1 devices are supported by the Clocks Tool:
MK21FN1M0AVLQ12 |
MK21FN1M0AVMC12 |
MK21FN1M0AVMD12 |
MK21FN1M0VLQ12 |
MK21FN1M0VMC12 |
MK21FN1M0VMD12 |
MK21FX512AVLQ12 |
MK21FX512AVMC12 |
MK21FX512AVMD12 |
MK21FX512VLQ12 |
MK21FX512VMC12 |
MK21FX512VMD12 |
MK22FN128CAH12 |
MK22FN128VDC10 |
MK22FN128VLH10 |
MK22FN128VLL10 |
MK22FN128VMP10 |
MK22FN1M0AVLH12 |
MK22FN1M0AVLK12 |
MK22FN1M0AVLL12 |
MK22FN1M0AVLQ12 |
MK22FN1M0AVMC12 |
MK22FN1M0AVMD12 |
MK22FN1M0VLH12 |
MK22FN1M0VLK12 |
MK22FN1M0VLL12 |
MK22FN1M0VLQ12 |
MK22FN1M0VMC12 |
MK22FN1M0VMD12 |
MK22FN256CAH12 |
MK22FN256VDC12 |
MK22FN256VLH12 |
MK22FN256VLL12 |
MK22FN256VMP12 |
MK22FN512CAP12 |
MK22FN512VDC12 |
MK22FN512VLH12 |
MK22FN512VLL12 |
MK22FN512VMP12 |
MK22FX512AVLH12 |
MK22FX512AVLK12 |
MK22FX512AVLL12 |
MK22FX512AVLQ12 |
MK22FX512AVMC12 |
MK22FX512AVMD12 |
MK22FX512VLH12 |
MK22FX512VLK12 |
MK22FX512VLL12 |
MK22FX512VLQ12 |
MK22FX512VMC12 |
MK22FX512VMD12 |
MK24FN1M0VDC12 |
MK24FN1M0VLL12 |
MK24FN1M0VLQ12 |
MK26FN2M0CAC18 |
MK26FN2M0VLQ18 |
MK26FN2M0VMD18 |
MK26FN2M0VMI18 |
MK63FN1M0VLQ12 |
MK63FN1M0VMD12 |
MK64FN1M0VDC12 |
MK64FN1M0VLL12 |
MK64FN1M0VLQ12 |
MK64FN1M0VMD12 |
MK64FX512VDC12 |
MK64FX512VLL12 |
MK64FX512VLQ12 |
MK64FX512VMD12 |
MK65FN2M0CAC18 |
MK65FN2M0VMI18 |
MK65FX1M0CAC18 |
MK65FX1M0VMI18 |
MK66FN2M0VLQ18 |
MK66FN2M0VMD18 |
MK66FX1M0VLQ18 |
MK66FX1M0VMD18 |
MK80FN256CAx15 |
MK80FN256VDC15 |
MK80FN256VLL15 |
MK80FN256VLQ15 |
MK81FN256CAx15 |
MK81FN256VDC15 |
MK81FN256VLL15 |
MK81FN256VLQ15 |
MK82FN256CAx15 |
MK82FN256VDC15 |
MK82FN256VLL15 |
MK82FN256VLQ15 |
MKL13Z32VFM4 |
MKL13Z32VFT4 |
MKL13Z32VLH4 |
MKL13Z32VLK4 |
MKL13Z32VMP4 |
MKL13Z64VFM4 |
MKL13Z64VFT4 |
MKL13Z64VLH4 |
MKL13Z64VLK4 |
MKL13Z64VMP4 |
MKL17Z128VFM4 |
MKL17Z128VFT4 |
MKL17Z128VLH4 |
MKL17Z128VMP4 |
MKL17Z256VFM4 |
MKL17Z256VFT4 |
MKL17Z256VLH4 |
MKL17Z256VMP4 |
MKL17Z32VDA4 |
MKL17Z32VFM4 |
MKL17Z32VFT4 |
MKL17Z32VLH4 |
MKL17Z32VMP4 |
MKL17Z64VDA4 |
MKL17Z64VFM4 |
MKL17Z64VFT4 |
MKL17Z64VLH4 |
MKL17Z64VMP4 |
MKL27Z128VFM4 |
MKL27Z128VFT4 |
MKL27Z128VLH4 |
MKL27Z128VMP4 |
MKL27Z256VFM4 |
MKL27Z256VFT4 |
MKL27Z256VLH4 |
MKL27Z256VMP4 |
MKL27Z32VDA4 |
MKL27Z32VFM4 |
MKL27Z32VFT4 |
MKL27Z32VLH4 |
MKL27Z32VMP4 |
MKL27Z64VDA4 |
MKL27Z64VFM4 |
MKL27Z64VFT4 |
MKL27Z64VLH4 |
MKL27Z64VMP4 |
MKL33Z128VLH4 |
MKL33Z128VMP4 |
MKL33Z256VLH4 |
MKL33Z256VMP4 |
MKL33Z32VFT4 |
MKL33Z32VLH4 |
MKL33Z32VLK4 |
MKL33Z32VMP4 |
MKL33Z64VFT4 |
MKL33Z64VLH4 |
MKL33Z64VLK4 |
MKL33Z64VMP4 |
MKL43Z128VLH4 |
MKL43Z128VMP4 |
MKL43Z256VLH4 |
MKL43Z256VMP4 |
MKS22FN256VLL12 |
MKS22FN256VLH12 |
MKS22FN128VLL12 |
MKS22FN128VLH12 |
In November, the following SDK V2.0 R2 and R3 devices will be available in the Clocks Tool:
MKL14Z32VFM4 |
MKL14Z32VFT4 |
MKL14Z32VLH4 |
MKL14Z32VLK4 |
MKL14Z64VFM4 |
MKL14Z64VFT4 |
MKL14Z64VLH4 |
MKL14Z64VLK4 |
MKL15Z128CAD4 |
MKL15Z128VFM4 |
MKL15Z128VFT4 |
MKL15Z128VLH4 |
MKL15Z128VLK4 |
MKL15Z32VFM4 |
MKL15Z32VFT4 |
MKL15Z32VLH4 |
MKL15Z32VLK4 |
MKL15Z64VFM4 |
MKL15Z64VFT4 |
MKL15Z64VLH4 |
MKL15Z64VLK4 |
MKL24Z32VFM4 |
MKL24Z32VFT4 |
MKL24Z32VLH4 |
MKL24Z32VLK4 |
MKL24Z64VFM4 |
MKL24Z64VFT4 |
MKL24Z64VLH4 |
MKL24Z64VLK4 |
MKL25Z128VFM4 |
MKL25Z128VFT4 |
MKL25Z128VLH4 |
MKL25Z128VLK4 |
MKL25Z32VFM4 |
MKL25Z32VFT4 |
MKL25Z32VLH4 |
MKL25Z32VLK4 |
MKL25Z64VFM4 |
MKL25Z64VFT4 |
MKL25Z64VLH4 |
MKL25Z64VLK4 |
MKW21D256VHA5 |
MKW21D512VHA5 |
MKW22D512VHA5 |
MKW24D512VHA5 |
In December, the SDK 2.0 R4 devices will be supported by the Clocks Tool:
MKV10Z16VFM7 |
MKV10Z16VLC7 |
MKV10Z16VLF7 |
MKV10Z32VFM7 |
MKV10Z32VLC7 |
MKV10Z32VLF7 |
MKV10Z128VFM7 |
MKV10Z128VLC7 |
MKV10Z128VLF7 |
MKV10Z128VLH7 |
MKV10Z64VFM7 |
MKV10Z64VLC7 |
MKV10Z64VLF7 |
MKV10Z64VLH7 |
MKV11Z128VFM7 |
MKV11Z128VLC7 |
MKV11Z128VLF7 |
MKV11Z128VLH7 |
MKV11Z64VFM7 |
MKV11Z64VLC7 |
MKV11Z64VLF7 |
MKV11Z64VLH7 |
MKV30F128VFM10 |
MKV30F128VLF10 |
MKV30F128VLH10 |
MKV30F64VFM10 |
MKV30F64VLF10 |
MKV30F64VLH10 |
MKV46F256VLL16 |
MKV46F256VLH16 |
MKV46F128VLL16 |
MKV46F128VLH16 |
MKV44F256VLL16 |
MKV44F256VLH16 |
MKV44F128VLL16 |
MKV44F128VLH16 |
MKV44F64VLH16 |
MKV42F256VLL16 |
MKV42F256VLH16 |
MKV42F128VLL16 |
MKV42F128VLH16 |
MKV42F64VLH16 |
MKV44F128VLF16 |
MKV44F64VLF16 |
MKV42F128VLF16 |
MKV42F64VLF16 |
MKV58F1M0VMD24 |
MKV58F512VMD24 |
MKV58F1M0VLQ24 |
MKV58F512VLQ24 |
MKV58F1M0VLL24 |
MKV58F512VLL24 |
MKV56F1M0VMD24 |
MKV56F512VMD24 |
MKV56F1M0VLQ24 |
MKV56F512VLQ24 |
MKV56F1M0VLL24 |
MKV56F512VLL24 |
MKV31F128VLH10 |
MKV31F128VLL10 |
MKV31F256VLH12 |
MKV31F256VLL12 |
MKV31F512VLH12 |
MKV31F512VLL12 |
We hope you will find this new release useful.
Thanks for designing with NXP!
I tried to use the web version of the tool, but it said "MCU is not supported." (Using KL26Z) The release notes available from the help menu does list the KL26Z series. Is it wrong? Where is the list of supported processors?
A list of supported processors would be good as well. Does not seem to support the KL16. Looks great though.
Additional devices will be populated on the server over the coming weeks. I see if I can get a list/roadmap of them and put it up here for reference.
Hi David,
KL16 and KL26 were part of the Kinetis SDK release 2 (see https://community.nxp.com/docs/DOC-329783). The data for the clocks tool for the SDK release 2 and 3 is expected to be available on the server after Oct. 26.
I have not seen the KE1x listed yet, digging on it...
The list of supported devices can be found here for all the tools:
Please, set the HSRUN power mode (Run mode settings). The RUN power mode does not support 180MHz core clock frequency.
Best Regards,
Marek Neuzil