Identifier on PTI of MKE06Z128VLK4.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Identifier on PTI of MKE06Z128VLK4.

870件の閲覧回数
patricemenet
Contributor I

When I put an identifier to a pin of PTI / GPIOC to initialize this pin, the file pin_mux.c is removed and I loss pin init for GPIOA and GPIOB. In addition, the file pin_mux.h is not finished.

Have you ever seen this problem ?

0 件の賞賛
3 返答(返信)

712件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello Patrice,

I guess you did not save the Config Tools configuration (*.mex file) when this problem occurs. Still, could you please attach here the *.mex file and spcify what exactly you entered as the identifier? This could accelerate the reproducibility of the issue.

Thank you,

Libor

0 件の賞賛

712件の閲覧回数
patricemenet
Contributor I

Hello Libor,

I have saved the .mex file before I want to generate the code. You will find attached the .mex file.

Bests regards,

Patrice.

0 件の賞賛

712件の閲覧回数
Lukas_Heczko
NXP Employee
NXP Employee

Hi Patrice,

thank you for reporting this issue. Attached you can find patch fixing the problem in MCUXpresso Config Tools v6 and MCUXpresso IDE 11.0.x. You can install it using following steps:

1. In MCUXpresso Config Tools go to File > Data Manager, in MCUXpresso IDE go to ConfigTools > Data Manager 

2. Choose Import... and browse to the attached archive

3. Select processors for which you want to apply the patch

4. Restart MCUXpresso Config Tools or MCUXpresso IDE

The fix will be included in next version of MCUXpresso IDE and Config Tools.

Regards,

Lukas  

0 件の賞賛