I believe there are a couple of bugs in the config tool when configuring SPI for LPC845.
If I select Clock polarity: CPOL=0: SCK inactive in low, the flag kSPI_ClockPolatityActiveLow is used which is the opposite behavior.
Also, If I want to transfer 8 bits of data I have to select "Data width [bits]" = 7. The configurator enters dataWidth = 7, but I assume kSPI_Data8Bits was supposed to have been used.
解決済! 解決策の投稿を見る。
Hello Terje,
Sorry for my mistake, yes, the issue still exit, I will report it to development team.
Thanks for your sharing.
BR
Alice
Hello Terje Mugaas ,
Which version of Config Tools and SDK do you used?
Please use the latest one, have fix these issue you mentioned.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Alice and thanks for you reply.
I am using the integrated Config tool in MCUXpresso IDE 11.0.0.
I just downloaded the latest version of MCUXpresso IDE 11.0.1 and the problem is still there. From the help menu, I see it is using ConfigTools Framework 6.0.0
The SDK is version 2.6.0 which is the latest available for the LPCXpresso845MAX board.
Where can I find the fix you mentioned?
Hello Terje,
Sorry for my mistake, yes, the issue still exit, I will report it to development team.
Thanks for your sharing.
BR
Alice