Tool for pre-flashing LPC546

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Tool for pre-flashing LPC546

2,169 次查看
jana_beck
Contributor II

Hello,

is there any device I can buy for flashing an MCU (LPC54606J512BD) before it gets soldered onto a PCB?
I am trying to save one step on the production line.

Thank you!

Jana

标签 (1)
标记 (2)
0 项奖励
4 回复数

2,091 次查看
brendonslade
NXP TechSupport
NXP TechSupport

Elnec have device programmers that include support for LPC546xx devices. They might have something for you: https://www.elnec.com/en/search/

 

0 项奖励

2,101 次查看
jana_beck
Contributor II

Hi Rong,
thank you for your answer.

I was hoping to find an off-the-shelf solution, but sounds like I have to design it myself.

So in total I would need:
- socket (to plug in the MCU)
- pull up resistors (puts MCU in ISP mode)
- connector for connecting an external flashing tool (like Flash Magic)
- I also need to power the MCU right?

Thank you,
Jana

0 项奖励

2,101 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jana,

Yes, there is not the  off-the-shelf solution, you have to develop the board yourself. On the board, the socket, pull-up/down resistors for the ISP pins, connector, power supply are required.

BR

XiangJun Rong

0 项奖励

2,101 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jana,

For production flash programming before it gets soldered onto a PCB, I suppose that you can develop a target board which integrates a socket which adapts to your package of LPC54606J512BD. After the flash is written, you can pop up the processor from the socket.

You can use the blhost tools or Flash magic tools to download code, in the condition, the processor must be in ISP mode.

Hope it can help you

BR

XiangJun Rong

0 项奖励