s32v234 not recognized Path

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32v234 not recognized Path

1,312 Views
willcampo
Contributor III

Hello everyone, I have already been able to configure the Matlab environment with the NXP.

But at the time I try to load the program "face_detection_camera_main" to the Board, I get the following error.

 

"C: \\ Users \\ waclab \\ AppData \\ Roaming \\ MathWorks \\ MATLAB" is not recognized as an internal or external command, program or batch file executable.

 

I have already tried adding the Path (as shown in the image) but in spite of that it does not work.

If you could help me, it would be very useful.

 

Path Error.png

Labels (1)
0 Kudos
Reply
1 Reply

1,182 Views
Daniel_Popa
NXP Employee
NXP Employee
0 Kudos
Reply