Will fsl-image-ubuntu be incompatible with s32v234sbc in the future?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will fsl-image-ubuntu be incompatible with s32v234sbc in the future?

3,413件の閲覧回数
feng_shuo
Contributor II

Dears

What machine is fsl-image-ubuntu currently compatible with? Where can I see a list of compatible machines? Will fsl-image-ubuntu be compatible with s32v234sbc in the future? When will it be supported?

Thanks

Shuo

ラベル(1)
0 件の賞賛
2 返答(返信)

3,297件の閲覧回数
Damienl
Contributor I


FSL is available ready to run for Mac OS X and Linux (Centos or Debian/Ubuntu) - with Windows computers being supported via the Windows Subsystem for Linux (WSL). We also provide source code if you run an OS not directly supported by us.

タグ(1)
0 件の賞賛

3,288件の閲覧回数
Damienl
Contributor I

Thanks for this reply bp credit card

タグ(1)
0 件の賞賛