S32V234 how to do communication between cortex A53 and Cortex M4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32V234 how to do communication between cortex A53 and Cortex M4

3,536件の閲覧回数
wubt01
Contributor I

Hi

How to do the communication between Cortex A53 and Cortex M4?
I am planning to use M4 to receiving the data form the peripheral device and than passing the message to the A53.
I am using S32V234 soc, dose this system has MCC (MultiCore Communication) or RPM (Remote Processor Messaging) Libs?
Could you please provide the suggestions and kindly tell me how to use this?

Thank you

BT

ラベル(1)
0 件の賞賛
4 返答(返信)

3,073件の閲覧回数
447825937
Contributor I

Hi ,

Have you find a solution for communicating with A53 and M4?  

I have a subject to use M4 for real time control which receive information from image process result on A53 then run real time controller on M4 . I have no idea about the communication part .

Is there any suggestions about that?

with great appreciate .

Thx.

0 件の賞賛

3,074件の閲覧回数
KushalShahNXP
NXP Employee
NXP Employee

Hi wubt01@gmail.com‌,

We do have Inter Core Communication(ICC) driver implemented on Linux  running on Cortex-A53 core and compatible AUTOSAR implementation that runs on Cortex-M4 core.

We are also planning to have compatible M4 FreeRTOS implementation(expected EAR in Dec 2018) that can talk with A53 running Linux.

Please refer to the Linux User Manual for more information on ICC.

Regards,

Kushal

0 件の賞賛

3,074件の閲覧回数
447825937
Contributor I

Hi , Kushal

Currently I find ICC only provide communications between A5x and A5x from the Linux User Manual . but I wonder if there is an example about  communication between A53 and M4 . it seems little material about this aspect . Any help would be appreciate !

0 件の賞賛

3,074件の閲覧回数
paulvlase
NXP Employee
NXP Employee

Hi kushalshah‌,

Do you know anyone that might be able to answer this question?

Thank you!

0 件の賞賛