HotFix: Vision Toolbox for S32V234 1.1.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HotFix: Vision Toolbox for S32V234 1.1.0

3,150件の閲覧回数
paulvlase
NXP Employee
NXP Employee

HotFix_1: "No function or variable is defined 'FileName'" error in nxpvt_build()

 

Problem: When trying to run run_face_detection_camera_main.m

 

Root Cause: Coding building error

 

Workaround:  Update the files attached in the following folders 

 {install_dir}\internals\build\private\nxpvt_build.p
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,933件の閲覧回数
jim_duan
Contributor II

I am using matlab R2018a. This hotfix doesn't work for it.

Thanks,

0 件の賞賛
返信

2,934件の閲覧回数
18502532079
Contributor I

well, the hot-fix seems not working, i encounter the same error When trying to run run_face_detection_camera_main.m

paulvlase

0 件の賞賛
返信

2,934件の閲覧回数
nxf40536
NXP Employee
NXP Employee

Hi 18502532079@163.com‌,

Can you please tell me which version of MATLAB you are using ? 

Thank you,

Vlad Dascau

0 件の賞賛
返信

2,934件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

iulianbulancea‌ 

nxf40536

Please have a look!

Thanks!

Daniel

0 件の賞賛
返信