"Transmit-only" mode on DPAA LS1046

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

"Transmit-only" mode on DPAA LS1046

456 次查看
holako92
Contributor I

A large variety of fiber ethernet PHYs and some copper ethernet PHYs support forced "unidirectional link" modes. Some signalling modes are designed for last-mile ethernet plants while others are designed for strict security isolation (fiber with no return-path). 

Unfortunately, this doesn't work with most NIC drivers even if sitting the autoneg off using ethtool. What would be the preferred way to set the TX only mode?

I look forward to your comments and suggestions

标记 (4)
0 项奖励
回复
1 回复

400 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Try powering the receiver (x00100000) or the transmitter (as asked) (x00080000) for the x1EA_0800 + 4 * lane m.

For example, for lane A, should be the address x1EA_0800

Best regards

0 项奖励
回复